This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

power-down with THS3095

Other Parts Discussed in Thread: THS3095

Hello,

I have problems with power down of THS3095. Regardless of level of voltage at pin 8 (nPD) - the device is always enabled (indicated by power consumption, voltage levels and amplifying function). At first: there is a single-supply situation.

The related voltage levels are: pin 4 = 0V (ground), pin 7 = +15V (positive rail), pin 1 = 0V (REF), pin 8 = 0V/+3.3V (nPD). Even if nPD and REF are at the same level (0V related to Ground) the device is activ - where it should be in power-down.

Any idea from someone?

regards

Karsten