Other Parts Discussed in Thread: OPA2544
I am currently simulating the OPA2544/544 as a Howland current source using TINA from the TI site. The model is correctly holding the current I am expecting at .6A with a 10ohm load. However, I am checking the total power consumption of the amplifier and I notice both inputs to the amp (+/-12v) are only consuming~ 5.22ma. This should be the bias current only. But according to the power required by the load (3.6W) the supply inputs should be consuming more than the above currents.
Is there a model issue or is there something I omitted?
Thanks,
Mike