Hello, I'm trying to simulate the LMV796/797 op-amp in SPICE and I'm running into a model where the op-amp rails on the positive end at 4.1V. It's a rail-to-rail amplifer, so I expected that rail to be higher. The negative rail is around 37mV, which makes more sense. Did anyone else have this issue? I used the PSPICE model from the LMV797 product page for this. Also tried this in Multisim (which has a model for it) and it also rails at 4.1V. Any help would be appreciated.