Hello,
I have a photodiode transimpedance amplifier made of a Hamamatsu S1226 photodiode and a IVC102 Burr-Brown integrating transimpedance amplifier. The amplifier is run in a reset-and-integrate mode with a integrating capacitor of 10pF. The integration time is 2,25ms.
My problem is that the amplifier circuit picks up 50Hz hum that decreases system performance. What would be the best way to minimize the unwanted hum? I have a PCB mounted shield box that covers the diode and the IVC102. The PCB trace between the photodiode and the IVC102 has a guard ring and is routed on the top layer. Is it better to place the trace one layer down so it can be shielded by ground planes above and beneath?
Does anyone have experiences on this matter?