I have a situation where we suspect LF147 needs measurement of its actual slew rate. it is used in die-form so I can only access pins taken out of the hybrid pkg. I have access to the most important section: the eror amp.Pin 12 is feeding a rectangular fast rising waveform through 4.99k, 13 to neg side of the signal is 4.99k. Feedback is 15k+470pf. Output is available through a 100 Ohm. I can vary amplitude. RIse time of pulse is 6ns.
How do I relate pulse response of this ckt to the slew rate of the opamp ?
thnx