Hi,
from the datasheet I have the impression, that the only difference between TLC393 and TLC7302 is the output stage. Is this true? In the datasheet of the TLC7302 it is written, that the input voltage may exeed Vcc without damage and without corrupting the output signal as long as the current is limited. In my application one input is connected to a 3V reverence, wheras the other monitors the voltage across a resistor. The resistor current is limited with a current limiting diode to less than 0.5mA. In this configuration the input voltage should be handeled correctly and without any damage to the device up to the voltage limit of the CRD. Is that correct? If TLC7302 and TLC393 are mainly identical this should also be correct for the TLC393. Is this assumption also correct or is there any difference in the input stage of the devices?
In the datasheet of the TLC393 on page 14 you can find "To maintain the expected output state, the inputs must remain within the common-mode range". Does this mean both inputs have to remain within the common-mode range or only one as for the TLC3702? The datasheet of this devices states on page 8: "Normal operation and correct output state can be expected even when the input voltage exceeds the positive supply voltage."
Best regards,
Dirk