This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ryuji Asaka,
Thank you for your interest in the INA220. I have a few questions about this application before I can decide if the INA220 is a good fit for it.
1. What frequency and amplitude is the AC waveform?
2. Is the +/- 10mA current riding on a larger current or would the shunt voltage be centered around 0V?
3. What is the Common Mode Voltage across the current shunt ("Supply" in the schematic you provided)?
4. The INA220 can convert at 9, 10, 11, and 12 bit resolutions at the cost of slower sampling rates. What is the target resolution of the application?
5. Is the goal to get an RMS current by taking sequential readings and calculating it, or simply to get a peak-to-peak current by constantly evaluating the measurement results?
6. What is the smallest current the customer expects to measure?
Thank you; I hope to help you with your application soon!
Jason Bridgmon
Ryuji Asaka,
Thank you for your answers. I have some suggestions and follow-up questions.
Ryuji Asaka,
After discussing the application a bit with a few other engineers, one suggestion for a different part that may be more suited to this application is the ADS131E04. This device can sample at 32kHz (more than the 20kHz needed for decent sampling of the input waveform) and has a built in PGA. With the PGA set to 12V/V, the number of bits of resolution is 11.3. The input impedance is 200MOhms, so 4.3ohms on it shouldn't be much of an issue.
This solution does have a few major differences, it is a serial interface and not an I2C interface, and it has substantially more pins and multiple power supplies. The customer may not be willing to accept this and possibly the price could be an issue as well, with the INA220 at about $1 US, and the ADS131E04 at $3.95 US.
Please let me know how else I can assist!
Jason Bridgmon
Ryuji Asaka,
This INA199A1 and ADC101C021 solution seems reasonable. I read up on the ADC101C021 and I see that it requires a stable Va because the power supply is also the reference to the device. In addition to that, the I2C bus is supposed to be pulled up to the same potential as Va, so the customer should take this into consideration when designing their circuit. See page 31 of the ADC101C021 for more explanation and application reference circuits.
The INA199A1 appears to be gain stable out to 10kHz and begins to drop off after that for a 15mV sine wave, which should satisfy your customer's requirements. Refer to figure 3, page 5 of the data sheet. At the bottom of page 9, the data sheet says that the INA199A1 operating on a 3.3V supply could easily handle a 60mV full scale shunt drop with only 150uV of offset. I believe this is more than adequate.
Jason Bridgmon