The TLV3401IDBVR is an open-drain output comparator, but the data sheet does not give any specifications for the max drain-source voltage for the output stage.
Question 1 -- Is the maximum output drain-source voltage the same as Vcc or is it a fixed value (20V, 30V, etc.)?
Question 2 -- Can the comparator be operated as a level shifter where the comparator is powered from 5V, but the output stage is pulled up to 15V?
Question 3 -- If so what is the maximum voltage that the output stage can be pulled up to?
Murdock Taylor
Electronic Product Design & Development Consulting Services (EPDDCS)