Hello!
I want to use ADS1675 for measurement 25 usec pulses with amplitude 2,5V and 2,5V offset. Pulse repetition frequency is 8kHz. I want to use fully differential Bessel filter on THS4131 (Gain = 1, Vcc=+5V, Vss=-5V). Can you check right amplifier choice for my application from THS4121, THS4120, THS4131 and THS4503? The criteria of choose is maximum SNR for pulses amplitude measurement.
P.S. You can suggest me another fully differential amplifier too.
With best regards, Maxim Galkin.