Dear All,
The datasheet of the TLV3492 specifies identical absolute max. supply voltage and upper limit for the operating supply voltage (5.5 V). Usually there is a certain margin for protection purposes and I was wondering, if there is an error in the datasheet or are the specs correct. If the latter is the case, which would be the recommended supply voltage?
Thanks and regards,
Silviu