Hello
I would like to know the value of the CMVR of LMH6644 as below specification.
The specification shows CMVR which are Min Typ Max in yellow color. The values are scattered from Min:1.8, 1.6, Typ: -0.5, 2.0, Max:-0.2, -0.1. I am very confused because which one is considers for designing.
1. Which Values is considered for design factor?
2. If the typical CMVR is -0.5V, is the input voltage limited as Vs-0.5V(V+=3V, V-=0V, Gain=1)?
Does the means that Violation VCM is 2.5V?