Hello,
I intend to use OPA2381 as a transimpedance amplifier for a photodiode (Everlight PD638B) in my project. The impendance of that photodiode is 333M (dark)....200K (1mW/cm²). In TINA-TI the amplifier doesn't work properly without bias voltage on the positive input, the output voltage is always about 17,7mV in this case.
If I apply a Vbias to positive input (0,5V) the amplifier seems to work (output 2.06V…4,59V). Could you please explain me the reason why Vbias is required? I attached a TINA-TI simulation file with the schematic.
Many thanks in advance.
Best Regards
VL