This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA690 Asymmetrical Power Supplies

Other Parts Discussed in Thread: OPA690

Hoping you can confirm this application.  Looking to power an OPA690 from +3.3V and -3.0V power supplies.  The application is a low speed cable driver where the high output drive and disable features are important.  

The amp is configured as a unity gain voltage follower with the + input DC coupled to the signal source.  The input signal is a 5KHz digital signal swinging from 0v to +3.3v.   TINA simulations all look fine.    Do you see any issues that may not have been reflected in the TINA model?

4064.ltc_tx_cct_design 3V3 op amp.TSC