Hi,
We want to use LMP8602 as a Shunt monitor over a active Shunt (MosFET). The supply of the LMP8602 is 5V.
We have a differential input voltage of 16V max. in fault condition. I didn't find any max ratings of the differential voltage in the datasheet.
The only thing I found is on page 14:
"The LMP8602/LMP8602Q/LMP8603/LMP8603Q use level shift resistors at the inputs. Because of these
resistors, the LMP8602/LMP8602Q/LMP8603/LMP8603Q can easily withstand very large differential input
voltages that may exist in fault conditions where some other less protected high-performance current sense
amplifiers might sustain permanent damage."
What does "large differential input voltage" means? Is there any max. rating specified I miss?
Thanks in advance!
Stefan