This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP8602 max differential input voltage

Other Parts Discussed in Thread: LMP8602, LMP8603

Hi,


We want to use LMP8602 as a Shunt monitor over a active Shunt (MosFET). The supply of the LMP8602 is 5V.

We have a differential input voltage of 16V max. in fault condition. I didn't find any max ratings of the differential voltage in the datasheet.

The only thing I found is on page 14:

"The LMP8602/LMP8602Q/LMP8603/LMP8603Q use level shift resistors at the inputs. Because of these
resistors, the LMP8602/LMP8602Q/LMP8603/LMP8603Q can easily withstand very large differential input
voltages that may exist in fault conditions where some other less protected high-performance current sense
amplifiers might sustain permanent damage."

What does "large differential input voltage" means? Is there any max. rating specified I miss?

Thanks in advance!

Stefan