This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA326 and 100mV reference voltage (using LM111)

Other Parts Discussed in Thread: INA326, LM111, LM7705, TIPD129

Hi Pete el al,

In this topic: 

We are using the INA326 device, to convert range (0V-5V) to (0V-3.3V). And in this version, we decided to ignore the non-linear region of output INA326.

And for preparing the next one, I want to update the schematic, so we can fully convert (0V-5V) to (0.1V-3.3V).

1. Solution 1: I use a LM111 device for creating the low reference voltage, please see the simulation attached file and help give me advice or suggest me a better device.

INA326_LM111.TSC

2. Solution 2: Can I supply the negave voltage for INA326 at V- pin, which means INA326 will be operated with +-5V, and the linear region of output will be widen. And the output will be linear in 0V-3.3V. Do you think this solution is okay for implement?

Thanks and Best Regards,

Hoang