This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM741

Other Parts Discussed in Thread: LM741

is LM741 work with +5 v and -5 v?

  • Hello Rushin,

    Yes, it will work. But the input range and output swing will be limited.

    The LM741 is not "Rail to Rail" in or out. So it needs some "headroom" on the input.

    The input range is specified at 2V from each rail, for a total valid input range of ±3V on a ±5V supply. The output swing will also be limited to ±4V.

    As long as your input and output signals are within those ranges, it should be okay.

    Regards,