This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Balance/Strobe pin & Balance pin of LM6511

Other Parts Discussed in Thread: LM6511, LM311-N

Hello.

I want to ask about pin5 and pin6 (BALANCE) of LM6511.

Please show the reference circuit doing offset adjustment with this balance pin.
And please tell connection when I do not use the balance pin.
Connect 5pin and 6pin directly, and do not do wrong movement?

By the way, there are few high-speed comparators in Wide VIN.
Therefore, the customer is going to choose this device.
If there is the device which I can recommend elsewhere, please show it.

Regards.

k.hashimoto.