Hi
I wish to use a OPA1652 to convert from a differential/balanced audio input to an unbalanced output (using a standard three op amp configuration as per circuit below to do this).
To ensure that the gains are correct through the system I require that the overall gain is set to 0.5 (ie in differential stage where R3=R2/2 from circuit below, Input buffers are unity gain).
Are you able to confirm that the OPA1652 will be stable with this gain of 0.5. Would also note that will be driving internal circuitry so load capacitance is minimal.
The data sheet states that stable for unity gain but am aware that phase margin reduced for successively lower gains.
I could look at implementing different configuration with inherent 0.5 gain but would prefer to use circuit shown below.
Thanks
Regards
Chris