This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can the LMH3401 be used to convert a differential signal to single-ended signal?

Other Parts Discussed in Thread: LMH3401EVM

Hello,


I have a differential output signal from an avalanche photodiode that I need to convert to single-ended output. The output range is +- 80 kV and the bandwidth is >2 GHz. Can I use the LMH3401EVM for that? If not, is there another solution?

Thanks.