Other Parts Discussed in Thread: OPA4322
Hi Dears,
Could you help to recommend one amplifier which is pin to pin with OPA4322AIPWR TSSOP package,
1) with similar performance, the bandwidth>5MHz is OK; 2) fit for Vcc=2.7-5.5V application; 3) The Vol at single power supply application can be as low as 50mV, 4) good small signal response, 5) but first of all, the supply current(four amplifier) should <4mA @Vcc=5V single supply.
Could you help to recommended one? Its urgent thanks!
BR,
Helen