Hello, I'm using 2 OPA353 for a 4th order filter. This op amp range from 2.7 to 5.5 for a voltage source. I also have a amplifier. Can I connect a same voltage source for both op amps? Let's say a 5V source for the two OPA353? Or a 15V for both op amps and the instrumentation amplifier? The amplifier voltage supply range from 5-15V. I'm new on this topic so I don't know much, suggestions are welcome.