Hello,
Our customer use NJU7047-T1 for Automotive application.
http://www.njr.com/semicon/PDF/NJU7047Automotive_E.pdf
I promoted OPA2322-Q1 for replacement.
But, the package size is little difference.
Are there any plan to release the VSP8 package of OPA2322-Q1 ?
Also, the customer request specifications are following.
Are there any competitive device without OPA2322-Q1?
VDD=5V single supply
Rail to Rail IN/OUT
GBW=5MHz(typ)
S/R=5V/us(typ)
Offset = 5mV(max)
drift =2uV/C(typ)
AUtomotive
-40C~+125C
Best Regards,
Ryuji Asaka