Other Parts Discussed in Thread: OPA335, IVC102
Hi,
I'm trying to design/test a photodiode integrator circuit for very low light levels. My circuit operates at low frequency. I simulated and am now testing several different op-amps, but I've run into issue with two chips. I've tried using an OPA335 amplifier and it does respond to different levels of light, but I can't get the signal to stop integrating/go to zero. The slope of the integration changes according to light conditions, but it never goes to zero (even under the same conditions that give no signal with other op-amps). The integration in what I think should be complete darkness the signal will still eventually go to saturation over the integration period that I'm using. I'm trying to figure out where this effect may be coming from. The only thing I can think of is some kind of charge injection due to the correction current for the zero offset op-amp. Or, possible some kind of noise effects. Does anyone have any thoughts? Thanks!