Hi guys
I'm trying to make a high gain amplifier which consists in two stages of 40dB each (x100). I'm using the OPA846 which should fulfill the gain requirements for at least 1 MHz bandwidth. The voltage input would be very low like 2 mV and would have offset, so it has to be compensated and that's why the positive input has a variable voltage reference.
The schematic is in the next image: By the way Vcc is 5V:
V1 should be the result of combining the two sources (correct me if I'm wrong), the input and the reference. V1 = 101 · V3 - 100 · V2 = 100 · ( 1.01 · V3 - V2 ) ~ 100 · ( V3 - V2 )
I've tested it with an oscilloscope probe and the results are in the next two images (sorry, I only have a two channel oscilloscope):
The screeshots were measured with 16 samples averaging to lower the noise.
Let's start with the second oscilloscope image, this screeshot shows the input (V2 in yellow) and the voltage reference in the positive input of the first stage (V3 in blue). As you see there is a little crosstalk in V3 which I don't know if would affect the proper behavior of the amp. The voltage reference is a lot greater than the input voltage, if I lower the reference a bit the output goes to zero and if I increase it the amp saturates to Vcc. Also the math channel (in red) shows V3-V2 which is the signal that the amp should amplify.
The first screenshot shows the input (V2 in yellow) and the output of the first stage (V1 in blue). The output should be the signal in red from the second image multiplied by 100 but it isn't.
Well, I'm a bit lost with that, could anybody explain what's happening?
Thank you in advance, by the way have a nice weekend.