about my problem: my application is a laser pulse detection, in this process when a laser pulse falls on photo diode it generates current, later stages include a I-V conversion, Gain,difference amplifier and comparator
about my pulse characteristics : pulse width
min
:10ns max
:150ns rise/fall time
:2ns-5ns pulse to pulse width
:22uS
How i selected the opamp for Gain and difference amplifier stages
key parameters: BW
- bandwidth and SR
- Slew Rate
from this literature i found my BW can be calculated by formula
BW
=0.35/(rise time
)=0.35/5ns=70MHz
Now slew rate is to be calculated
SR
= 2 * 3.14* BW
* Vp
= 2 * 3.14* 175MHz *4V = 2198V/us
qualifiying above requirements one such opamp is THS3001, with much better slew rate and BW
Please find the design file attached, which makes uses of THS3001, why am i not able to achieve the desicribed gain, i took the spice model given by TI and simulated it, stil i am not able to view proper output, why so ?