Dear all,
I would buy the evaluation board evm INA 282-286. what is the maximum rating current supported by the board?
do you think it supports a maximum current of 5 A?
Thanks in advance for any comments!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
I would buy the evaluation board evm INA 282-286. what is the maximum rating current supported by the board?
do you think it supports a maximum current of 5 A?
Thanks in advance for any comments!
Hi Carmine,
The PCB traces on the board are 40mil and using a PCB calculator(you can find anywhere on the web) you could go up to approximately 2.4A and go up 10 degrees C. You can also use an external shunt and not run the current through the PCB and just sense the voltage with the EVM.
Regards,
Javier