This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS9001

Other Parts Discussed in Thread: THS9001

Hi,The THS9001 's DC supply is 3V to 5V and it's 1-dB compression at 350 MHz is 20.6 dbm.

The 20.6 dbm at a 50ohm-load  is about 6.77Vpp.

Could it outputs above the DC supply(5V) when the load is 50 ohm?