Hello-
We'd like to use the LMH5401 to receive a single-ended input from 0 to -1V, with fast negative-going pulses into a 50 Ohm termination resistor. We want to invert the signal so that we can feed into a high speed ADC, with a gain of -1.5V/V.
Figure 60 in the data sheet shows a possible solution, and the gain is described as 4V/V. But isn't it actually -4V/V, since the input is fed to the inverting input of the amplifier?
Thanks and Best Regards,
-Tim Starr on behalf of GG@ES