I have designed a 3 Op Amps instrumentation amplifier with a variable gain (potentiometer) from 1V/V to 10,000 V/V . It seems to work fine in the simulations (TINA TI) with Op amps that are dual supply, but the problem is that I'm limited to build this with a positive single supply of 5V. I've tried different op amps single supply rail to rail, but they seem to not work at low input voltages.
For example, If I put a 0.1V and 0.08V with a gain set to 100V/V, the reference value will be 0.02V multiplied by 100V/V. The expected output should be 2V, but I don't see this. The output values are really small and sometimes they don't even amplify at all. The problem is with low input voltages.
*Note: Both input voltages are DC, not AC.
Any advice on what should I be looking at? Any suggestion will be appreciated,
Thanks!