Dear TI engineer.
I have a few questions.
1. If the surface temperature of the LM324N of 61 ℃ (@ ambient temperature of 24 ℃), can I see that the LM324-N is normal behavior?
2. Do you have a guide that will be sure how much (Absolute Maximum Ratings) ?
3. What if you use both the tying Output 4 channels of LM324-N to allow the current upper limit is how much?
4. Is the TI technical proposal to lower the surface temperature of the LM324-N?