Hello,
Our customer uses the TLV333, has an issue.
The customer are using the TLV333 as follows.
circuit : non-inverted amplifier
VCC=3.4V
amplitude : 261 times
pre-filter : RC low pass filter as R=10kohm, C=1uF at +input
The issue is that the output voltage is High (3.4V) when the input voltage is GND.
It need more than 1uA of bias current for the output voltage is High.
Is it possible to flow a bias current such as large value?
Best Regards,
Naoki Aoyama