This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLE2142 and TL3472 - single supply

Other Parts Discussed in Thread: TLE2142, TL3472

Hi all

Would you mind if we ask TLE2142 and TL3472?

Our customer would like to use TLE2142 and TL3472 with single supply 0V to 36V.
Is it possible?
Because we can't find VS=(Vcc+) - (Vcc-) on Absolute Maximum Rating.

We need your help.

Kind regards,

Hirotaka Matsumoto

  • Hello Hirotaka,

    The TL3472 has VSupply AbsMax of 36V. However, it is usually not recommended to operate a part at its AbsMax supply rating, since at 36V operation, even small surges in the supply voltage can damage the part.

    The TLE2142 has an VSupply AbsMax of 44V, so it can be used with a single supply of 36V.

    Best Regards,
    Mihir Gupta
    Field Applications Engineer,
    Texas Instruments