This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3001 max supply voltage

Other Parts Discussed in Thread: THS3001

The THS3001 datasheet shows 37V as both the abs max supply voltage as well as the max recommended operating.  Seems abs max should be higher than max recommending operating.  Is one of these wrong?

  • Hi Peter,

    This is a specail case, the THS3001 has a high voltage option which is tested to provide for a maximum operating voltage that is the same as the absolute maximum voltage.

    If you do decide to run the maximum supply voltage it will be important to make sure that the power supply is well regulated and has no high voltage glitches.

    Regards,
    Loren