When I simulate the THS3001 configured as unity gain with 1K feedback resistor, I get a weird glitch on the input waveform. My input is 2V swing with 10ns edge driven from a 50-ohm source, and my supplies voltages are +31.5V/-3.5V. If I reduce the input swing or supply voltage, it reduces the glitch. Is this glitch real?