I have a laser driver current clamp circuit utilizing the OPA378. During DVT testing I discovered this part suffers from an increased input bias current (increases into the uA range) when the input differential voltage exceeds roughly 750mA. This is a definite problem for my design because I can have an input differential voltage as high as 1.75VDC. The prototype boards are done so I'm trying to find a package and pin compatible drop in replacement part that doesn't have this issue. I think I have found a part that might work - OPA316IDCKR. However, the datasheet doesn't give any information about the input bias current versus differential voltage. Can anyone tell me this information? The OPA378 shows it in the application section of the datasheet but I missed it during my initial design. The fact that this type of information is missing in the OPA316 datasheet could mean (and I hope it means) that this part doesn't suffer from this issue. The input bias current for the OPA316 is listed in the electrical characteristics section as +/-15nA over the entire temp operating range which would be good enough for me. Thanks for any help!