Hi,
I am using LF356MX op-amp in design. I am operating LF356MX with 5V supply.
I have following queries related to this part:
1) As per datasheet, maximum current required for LF356 is 10 mA @±15V supply. So, what will be current @±5V supply?
2) Can this op-amp operate with single supply (i.e. 0 to 5V) instead of ±5V?
3) As per Recommended operating Conditions, LF15X can be operated between ±15V to ±20V supply but as per graphs (typical DC performance characteristics), LF155/6 are shown to be operated with ±5V, ±10V, ±15V and ±20V. So, can i use LF155 with ±5V supply?