Hello,
The purpose of our system is to measure a 80VAC signal generated by an independent power supply (Totally different ground) , and convert it into a -/+ 10 Vac signal suitable to be analyzed .
This power supply is a Sinus 80VAC MAX , 400 HZ , but why have no idea about the common mode .
We wanted to try a classic difference amplifier with a Gain of 0.125 , powered by an isolated DC/DC converter but , we don’t know if the voltage on the input pins are acceptable because of common mode .
Beside we need a 1Mohm input impedance ( at least ) .
We tried this circuit but we had some oscillations noises because of the too large feedback resistance. And the internal features of this OP AMP
Do you have a better solution or another kind of OPAMP more suitable to do the JOB
Thx
Regards
CSD17585F5