This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA220-Q1: bias and offset current

Part Number: INA220-Q1
Other Parts Discussed in Thread: INA226, INA220EVM

Hi team,

In the datasheet, we have only these following details:

« Iin+, Iin- Input bias current at IN+ and IN-« (Ta=25°C, active mode, Vin+ = 12V ; (Vin+ - Vin- ) = 32mV, PGA=/1) typical = 20µA

Could you provide me the Ibias and Ioffset under these conditions:

  • Ta=85°C
  • Active mode
  • Vin+=320mV
  • Vin- = 0V
  • PGA= /8
  • Maximum value

Thanks in advance for your help.

Pol