Other Parts Discussed in Thread: ADC34J45, , LMH6521, TIDA-00073, ADS41B49, TINA-TI
Hello,
My design will include the ADC34J45 that will have JESD204B interface to ALTERA ARRIA 10 FPGA.
The four analog inputs will be amplified by the LMH6522 amplifier.
There are 2 frequency possibilities of analog signal inputs 189MHz or 236MHz.
The analog inputs parameters are :
- single ended
- Frequency: 189MHz or 236MHz.
- BW: 30MHz
- 50 Ohm.
The sample rate is 108MHz or 135MHz (Nyquist4) respectively to the input frequency.
Can you please advise what is the recommended impedance matching between the LMH6522 and the ADC34J45 and the recommended impedance matching between the
single ended input signal (50 Ohm) and the LMH6522?
Thank you,
David Siksik