This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP7721: LMP7721 about the output voltage issues

Part Number: LMP7721


Hi Team,

The customer is using LMP7721. The attachment is his schematic. R10 is 10M. R9 and R11 is 0 ohm. C18 is unconnected.

The APD device can provide the current for  LMP7721. The IN- pin input current that the APD device provides is about  tens nA to hundreds nA.

When the  IN- pin input current is changed, the output voltage for LMP7721 is always colsed to  +2.5V.

What is the reasons? How to solve the issue?

Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments