The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA330: temperature coefficient of current conveyor

Part Number: INA330

The INA330 datahseet specifies the maximum variation across -40 to +85 degrees C of the current conveyor offset, which is the dominant source of instability. I would like to know what the temperature coefficient of this error is. Is it likely the variation is linear across the -40 to +85 range? My applications will only ever expose the INA330 to a narrow range  around room temperature in a well controlled lab, but requires the best possible stability.

Thanks, Jochen

  • Hello Jochen,

    Sorry we have been slow to answer; there has been a lot going on.

    The INA330 datasheet only assures that the Current Offset Error Change Over Temperature from +25°C to +85°C, or +25°C to –40°C, will be no greater than ±40 nA. It doesn't provide specific limits for the parameter's stability, or temperature coefficient, and it must be assumed to be able to drift in either direction.

    The "CURRENT CONVEYOR OFFSET ERROR CHANGE OVER TEMPERATURE PRODUCTION DISTRIBUTION" graph on datasheet page 5 indicates that over a wide temperature range the offset error can be positive, or negative; however, the distribution is weighted to the positive. Likely, in a relatively temperature stable environment any error in the current due to a temperature change will be a very small fraction of the change observed over the +25°C to +85°C, or +25°C to –40°C, temperature ranges.

    Regards, Thomas

    Precision Amplifiers Applications Engineering