Part Number: TLV2402
Hi,
We are using a TLV2402IDR in a battery balance circuit and VCC is connected to +12V and GND is connected to ground in our setup. While testing the board, the amplifier was outputting +4V and when a tech probed the board to look at a signal, pin 8 (VCC) was shorted to pin 7 (OUT) momentarily. I could not specifically find a mention of output short circuit protection for this device, so I am not sure if the part was stressed at all. It appears to still be working fine, but we will replace it if there is any possibility of damage. I have read that other amplifiers have protections such that any short to a voltage between VCC and ground is OK, but if you exceed VCC or GND there may be damage.
Thanks for any information,
Gary Gravante