Part Number: PGA112
Hello:
Really hoping I can get some help on this issue. Using a PGA112, connected as shown in the attached image, "PGA112_Connect.jpg"
Vdd is at 3.3V, Vref is at midpoint of 1.65, and connected to PGA112's vref input. If I am using CHN1, I would then expect the DC at the output to be at Vref. For whatever reason, and no matter what I write to the PGA112, the output wants to stay at Vdd. Please refer to the other attached images, PGA112_CS_CLK and PGA112_CS_DATA. I have divided down the SPI interface prescaler by 64 to allow eons of time for setup and hold delays, etc. Everything appears to be good. I am writing 0x2A12, which (from pg.27 of data sheet) is WRITE and CHN1 selection bit.
Can anyone see a problem...thanks for your help!