This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR117: Failed on field O/P 0A

Part Number: XTR117


Dear Sir,

We are using XTR117 as a V to I (4 to 20) convertor.

AC voltage from the field (0 - 2.5 Vac) is applied to an Op-Amp based circuit which converts it to (0 - 5Vdc) DC.

This voltage is given as an input to XTR117 to obtain 4-20.

This device is used with a testing set-up for 3 Phase CTs and Overload relays (3 devices used for 3 phases each). current in the range of 10-1200A is passed through these CTs/Overload Relays and their O/P which is 0-2.5Vac is input to this OpAmp based circuits and further to XTR117.

One fine day, when the set-up was turned on, 2 out of 3 devices failed and o/p was 0A. On replacing XTR117, desired o/p was obtained.

In order to investigate the cause of failure, we shorted I/P of Op-Amp ckt. However, o/p of 4mA and not 0A was obtained.

We are not able to determine the cause of failure.

Can you please suggest a possible cause and guide us how to go about troubleshooting so that we can take precautions.

My email Id is komal.hm@gmail.com. Please mail me in case you want the schematic so that I can revert.

Thanks,

Regards,

Komal Marathe.