Part Number: THS4524
Other Parts Discussed in Thread: ADS1278
Hi,
If the THS4524 is unpowered, what is the maximum safe voltage that can be applied to it's /PD pins? I'd like to be
able to allow 3.3V, but am worried that could damage the part. Not sure if this pin has protection diodes and how they would react. I
am able to limit current to well below 1mA (likely below 0.1mA) as the voltage on this pin is governed by a weak pull-up resistor to 3.3V.
Thanks, Dan