Other Parts Discussed in Thread: LM339, TLV3704
Hi,
My customer is using LM339-N.
He has questions about input voltage range.
Condition is V+ = 5V and V- = GND.
Q1: Can we use LM339-N with INPUT+ = +1V~+9V(swing signal) and INPUT- = +3.5Vdc(fixed value (REF)) at this condition?
Q2: Can we use LM339-N with INPUT- = +3.6Vdc(fixed value (REF)) at this condition?
Best regards,
Shimizu