Good afternoon all!
I'm reviewing a design for a colleague and I noticed a couple of things that could use some answers.
1) What is the US Government Cage Code for TI with respect the to the OPA2320? When I search "Cage Code, Texas Instruments", I get several different Cage Codes, and I assume that is because the different TI groups took out different ones as they formed. Whatever the case, if someone knows the correct Cage Code for the TI that makes these parts, I'd appreciate it. I don't believe this is a QPL/QML listed part.
2) What is the top-end temperature for this device? Our design requires the top-end temperature range to be +150C ambient with a very low power in extreme circumstances. The data sheet states that the operating range is -40C to +125C in several places, but then it states in Section 6.1 for the Absolute Maximum Ratings that the Operating Range is +40C to +150C. Additionally, Digikey seems to think that the OPA2320AIDGKR is only rated to +125C, while the OPA2320AIDGKT is rated to +150C.
Your help in nailing down these issues is appreciated.
-Tim