Other Parts Discussed in Thread: LMV341
Dear all,
Could you teach me about the specification of VICM at V+=5V?
You define that Typ: -0.2~4.2V and Max: 4V.
Why maximum value is lower than typical value?
In addition, this specification is defined with Ta=25C, so the 4V is also typical value.
How should I think about these tipical value?
And, what is the maximum value over full range?
Best regards,