This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL3472-Q1: Slew rate variations

Guru 20090 points
Part Number: TL3472-Q1
Other Parts Discussed in Thread: TL082-Q1

Hello,

Could you please let me know the slew rate variation of the following conditions?

1. Slew rate vs. Vcc+=10V to 16V, Vcc-=0V 
2. Slew rate vs. temperature (Ta=-40C to +125C)

Best Regards,
Ryuji

  • Ryuji-san,

    I do not have slew rate data at different VCC or temperature.
    I was able to find slew rate trends for the base die in TL3472-Q1. From that I'd expect slew rate to drop by 33% at 125C at 30V and have no data for lower voltages.

    If min slew rate was important, I prefer TL082-Q1 over TL3472-Q1